This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to simulate INT0 external interrupt in CCS

hi all,
im unable to generate INT0 interrupt in simulator(using ccs 2.0 version) after doing the
"PIN CONNECT" specified in help (Tools --> Pin connect) and the input .dat file
has 55 85 99 rpt 111|EOS data,i could not see the INT0 ISR being served while Timer_ISR is
being served as xpected how could generate the INT0 interrupt in simulator mode and cross
check it..?

Thanks,
Ganesh