This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640: Can't install TI-RTOS into CCS

Part Number: CC2640

Tool/software: Code Composer Studio

I'm running CCS 6.2.0.00050 on Windows 10 and trying to install TI-RTOS 2.18.0.3 (for 13xx and 26xx).  TI-RTOS is in its default location, under C:\ti.  I go to Window->Preferences, select CCS->Products and click the Rediscover button.  In addition to several versions of xdctools, it shows C:\ti\tirtos_cc13xx_cc26xx_2_18_00_03, but it's grayed out with a red X in front of it, and I can't select it to install.  If it matters, both CCS and TI-RTOS were previously installed and working on this PC.  I ran into a build problem that I couldn't resolve, so I ended up uninstalling and reinstalling everything (CCS, BLE SDK and TI-RTOS).