Part Number: CC2640R2F
Tool/software: Code Composer Studio
I have a problem to download/install SimpleLink Academy in Version V1.14.2.04.
I installed Code Composer Studio 7.3.0.00019 and SimpleLink™ CC2640R2 SDK.
Then I downloaded ProjectZero from the TI CLoud to generate and run it in Code Composer Studio.
When trying to build the project I get gollowing message:
**** Build Finished ****
Buildfile generation error occurred..
Product 'com.ti.SIMPLELINK_ACADEMY_CC2640R2SDK' v1.14.2.04 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
Seems I have to install "simplelink academy cc2640r2sdk v1.14" in addition to SDK 1.50, but where I can download it?
Found no download option for version 1.14.
The download button in Ti Resource Explorer is not working.