Part Number: CC3200-LAUNCHXL
Other Parts Discussed in Thread: CC3200,
Tool/software: Code Composer Studio
Hi,
I am trying to program my CC3200 using external debugger(Blackhawk XDS100v2 JTAG emulator).
I gave connection to XDS100v2 and JTAG of CC3200 as per the pin-out mentioned in the following image(Highlighted block 2).
While doing the test connection using CCS I got the error log:
-------------------------------------------------------------------------------------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Jul 21 2017'.
The library build time was '19:36:41'.
The library package version is '7.0.48.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-180' (0xffffff4c).
The title is 'SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
---------------------------------------------------------------------------------------------------
I checked voltage at pin VTRef and it is zero. I don't get it what is the mistake. Please guide.
Regards,
Abhijit.