Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
I'm trying to build the enet_s2e application (spma072) with the Code Composer Studio version 7.3.0.00019 and the Tivaware_C_Series version 2.1.4.178 and I have plenty of errors. Is there anything I need to chance to make the build successful without errors? I'm using the EK-TM4C1294XL Launchpad. Thanks for any advice.
Description Resource Path Location Type
gmake: *** [config.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [enet_fs.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [enet_s2e.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [idle_task.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [lwip_task.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [serial_task.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [telnet.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/croutine.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/list.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/portable/CCS/ARM_CM4F/port.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/portable/MemMang/heap_2.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/queue.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/tasks.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [third_party/FreeRTOS/Source/timers.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [utils/locator.obj] Error 1 enet_s2e C/C++ Problem
gmake: *** [utils/lwiplib.obj] Error 1 enet_s2e C/C++ Problem
gmake: Target 'all' not remade because of errors. enet_s2e C/C++ Problem