Hi Champs,
We find there're 'call" instruction in the assembly files which is generated by the compiler tools. We did not find the detail usage in the spru732 document for example the delay cycles.
Below are one extract from assembly file generated by compiler tools. Looks the delay slot is 3 ?
Case1:
CALL .S1 _BsamGetHData1Zone_Opt ; |264|
MV .L2X A11,B4 ; |264|
ADDKPC .S2 $C$RL4,B3,2 ; |264|
MV .L1 A8,A4 ; |264|
|| ADD .S1X 8,SP,A6 ; |264|
|| MV .L2X A12,B6 ; |264|
$C$RL4: ; CALL OCCURS {_BsamGetHData1Zone_Opt} ; |264|
;** --------------------------------------------------------------------------*
B .S1 $C$L26 ; |264|
|| ADDAD .D1 A12,8,A4 ; |268|
LDW .D1T1 *A4++,A3 ; |275|
LDW .D1T1 *A4++,A5 ; |275|
LDW .D1T1 *A4++,A8 ; |275|
LDW .D1T1 *A4++,A7 ; |275|
LDW .D1T1 *A4++,A6 ; |275|
; BRANCH OCCURS {$C$L26} ; |264|
Thanks in advance!
Jane