Part Number: TMS320F28335
Tool/software: TI C/C++ Compiler
hi, i have some tunable parameters that i would like to place them in a separate memory for easy management. since the number of such parameters may change, i didn't create a separate section for each of them but just to place them all in one .paramData section in the flash.
the process of adding such params is automated in script.
i would like to capture if the data structure change so that the program always matches the structure.. but for the reason of simplicity i cannot use struct, which only generates one symbol.
if i add one param, it seems the linker placements are changing.. not by any order i can predict.
is there a way to "predict" what triggers the linker to place a particular data/var in the section of memory it is allocated for?
complicated question.. hope this is clear enough to solicit some ideas.
thanks
regards
gz