This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 V4.2 Debug Session Initiation Causes OMAP-L138 Experimenter to Reset

Guru 15580 points
Other Parts Discussed in Thread: OMAP-L138

When starting a debug session using CCS4 V4.2 the OMAP-L138 Experimenter board seems to be reset causing loss of connectivity from my serial connection to the C6748 DSP on the SOM (the connection to the C6748 DSP in the OMAP-L138 must be made through a serial port on the Experimenter board by interrupting the boot sequence and entering the U-boot portion of the firmware) . If I then unplug the XDS100 v1 USB emulator connector, then re-insert it, I can re-establish the serial port connectivity and enter the debug session. It appears as though CCS4 V4.2 is sending some sort of USB reset to the board when it first enters a debug session.

Can anyone shed light on this?

Thx,

MikeH