Other Parts Discussed in Thread: UNIFLASH
Tool/software: Linux
Hi all, i am on Fedora 27, i was using Uniflash the same versionin the same PC with the Fedora 26 and it was working, i have also installed in another computer with the Fedora 27 and it worked but now this is what is happening. I have searched throw the web but with no success. Please i need some help.
Best Regards
Here is the result from the command
sudo ./uniflash_sl.4.2.1.1562.run
[sudo] password for nicholas:
No protocol specified
No protocol specified
No protocol specified
No protocol specified
----------------------------------------------------------------------------
Welcome to the UniFlash Setup Wizard.
----------------------------------------------------------------------------
Please specify the directory where UniFlash will be installed.
Installation Directory [/opt/ti/uniflash_4.2.1]:
----------------------------------------------------------------------------
Setup is now ready to begin installing UniFlash on your computer.
Do you want to continue? [Y/n]: Y
----------------------------------------------------------------------------
Please wait while Setup installs UniFlash on your computer.
Installing
0% ______________ 50% ______________ 100%
#########################################
----------------------------------------------------------------------------
Setup has finished installing UniFlash on your computer.
Create Desktop Shortcut [y/N]: y
Launch UniFlash [Y/n]: Y
[21897:0111/170351:ERROR:browser_main_loop.cc(162)] Running without the SUID sandbox! See code.google.com/.../LinuxSUIDSandboxDevelopment for more information on developing with the sandbox on.
No protocol specified
[21897:0111/170351:ERROR:browser_main_loop.cc(208)] Gtk: cannot open display: :0
[21899:0100/000000:ERROR:zygote_linux.cc(587)] write: Broken pipe