Tool/software: Code Composer Studio
I have installed CCS 7.1.0 and i am importing a program which was build in CCS 3.3. The program imports . But while building, it says :make not found in path" . i have tried to change the CCS workspace but that did not help. i have also tried to change the Project> properties> CCS build "use default build command". But thie default build command option cannot be checked. in previous threads i read that the "make not found" problem was supposed to be resolved in CCS 5.5 onwards. i am using CCS 7.1 please suggest some help