Part Number: CC2640R2F
Tool/software: Code Composer Studio
1. Do you provide functions (in C or C++) to read in signals from input pins of the board? How do I include these functions into my C program?
2. After writing my program, how do I compile it into code for the onboard processor? I can run CCS and create a C program, but I don't see any way in CCS to compile it. Do I use SCSWhere can I find an example that does this? What tools do I use to do this?
3. When my program is ready and compiled, how do I flash (write) it onto the board? Where can I find an example that does this?
4. Once the program is on the board, how do I cause it to execute?
5. What functions do you provide to put the program into sleep mode to preserve power? How do I cause the program to come out of sleep mode at a chosen time? Can I send a command via Bluetooth from my PC or iPhone to wake up the board processor? Where can I find an example that does this?
I am thinking that I need some combination of the “CCS” (Code Composer Studio), “SCS” (Sensor Control Studio), and SDK to do these things.
I am further thinking that the “Project Zero” example for CC2640R2 is what will help, but your example here:
dev.ti.com/.../
does not help much - to begin with, I can't find the sample code.
Are there other places in your documentation that separately address each of the above tasks (1-5) and provide examples of doing them?