I am working on a EVM6472 demo board, and was using the onboard debug/emulation just fine. I wanted to speed up code download, and debug speed when using RTA, so I connected the Spectrum Digital XDS510 Plus USB. After creating a new taget config, and attempting to debug, CCS now crashes.
CCS Version: 4.1.3.00038
I have run the automatic update tool, but it claims everything is up to date.
From other posts, I read to add the TI_TRACE_LOGGER = 6 to the environment, and then attach the files in the ccsv4\emulation\analysis\bin\db directory
The real nasty part now is that both the onboard emulator and the Spectrum 510 crash CCSv4.