Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
Hello,
I am using CCS 7.4.0. I have imported Heart rate project from the location "C:\ti\simplelink\ble_sdk_2_02_00_31\examples\cc2650em\heart_rate\ccs" and I changed preprocess include
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Failed Board Reset: (Error -600 @ 0x0) A required dynamic library could not be located. The library isn't on the search path. (Emulation package 7.0.100.0)
IcePick_C: Error connecting to the target: (Error -600 @ 0x0) A required dynamic library could not be located. The library isn't on the search path. (Emulation package 7.0.100.0)
If I download simple_peripheral project from the location "C:\ti\simplelink\ble_sdk_2_02_00_31\examples\cc2650em\simple_peripheral\ccs" it is downloding without errors and working fine.
Kindly help me to download the heart rate project in CC2650 Launchpad.
Thanks & Regards,
Murali.M