Other Parts Discussed in Thread: TMS320F28335, C2000WARE
Hi all,
I am experiencing similar issues with CCS 7.4.0 for Mac OS. I installed everything new (since I had not yet installed any previous versions or projects) and tried to run the LED blink sample code for the TMS320F28335 on the Delfino C2000 experimenter kit. In the end, I got the program to run on the F28335, but running the Debugging probe via either XDS100v1 or XDS100v2 took very very very long: approximately 20 minutes (for just running the example code). During this, the interface was buggy/laggy/not responding at all. Buttons like 'Run in Background' etc were not working at all. Especially the 'GEL Expression: OnReset(0)', 'GEL Expression: OnTargetConnect', and in the end the 'Loading Program' took very long.
If there are any ideas to speed this up, would be very helpful. I am now trying to install CCS v6, to see if it is CCS version specific, or has to do with any USB drivers, or has to do with the experimenter kit itself.