Other Parts Discussed in Thread: CCSTUDIO
------------------------------ hab1.pjt - Debug ------------------------------
[main_dma1.c] "D:\CCStudio_v3.1\C5500\cgtools\bin\cl55" -g -fr"D:/Projects/hab1/Debug" -i"d:/CCStudio_v3.1" -d"CHIP_5509A" -@"../../../../../../Projects/hab1/Debug.lkf" "main_dma1.c"
"main_dma1.c", line 59: warning: nonstandard conversion between pointer to function and pointer to data
"main_dma1.c", line 61: warning: nonstandard conversion between pointer to function and pointer to data
[Linking...] "D:\CCStudio_v3.1\C5500\cgtools\bin\cl55" -@"Debug.lkf"
<Linking>
>> warning: creating .stack section with default size of 500 words.
Use
-stack option to change the default size.
>> warning: creating .sysstack section with default size of 500 words.
Use
-sysstack option to change the default size.
>> warning: creating .sysmem section with default size of 1000 words.
Use
-heap option to change the default size.
Build Complete,
0 Errors, 5 Warnings, 0 Remarks.