This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: Build error simple_peripheral example

Part Number: CC2640R2F

Tool/software: Code Composer Studio

I get an error building simple_peripheral_cc2640r2lp_app.

I installed the project using resource explorer, which also installed simple_peripheral_cc2640r2lp_stack_library

With  simple_peripheral_cc2640r2lp_app selected in the Project Explorer window, I do a build and get this error:

"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 2 all -O

'Building file: "../TOOLS/app_ble.cfg"'
'Invoking: XDCtools'
"C:/ti/xdctools_3_50_04_43_core/xs" --xdcpath="C:/ti/ccsv7/ccs_base;C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source;C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/kernel/tirtos/packages;C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.simplelink:CC2640R2F -r release -c "C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS" --compileOptions "-mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path=\"C:/ccs_workspace/simple_peripheral_cc2640r2lp_app\" --include_path=\"C:/ccs_workspace/simple_peripheral_cc2640r2lp_app/Application\" --include_path=\"C:/ccs_workspace/simple_peripheral_cc2640r2lp_app/Startup\" --include_path=\"C:/ccs_workspace/simple_peripheral_cc2640r2lp_app/PROFILES\" --include_path=\"C:/ccs_workspace/simple_peripheral_cc2640r2lp_app/Include\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/controller/cc26xx_r2/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/rom\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/common/cc26xx\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/examples/rtos/CC2640R2_LAUNCHXL/blestack/simple_peripheral/src/app\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/icall/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/profiles/dev_info\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/profiles/roles/cc26xx\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/profiles/roles\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/profiles/simple_profile/cc26xx\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/profiles/simple_profile\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/target\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/hal/src/target/_common\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/hal/src/target/_common/cc26xx\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/hal/src/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/heapmgr\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/icall/src/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/osal/src/inc\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/services/src/saddr\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/services/src/sdata\" --include_path=\"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/devices/cc26x0r2\" --include_path=\"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.6.LTS/include\" --define=DeviceFamily_CC26X0R2 --define=BOARD_DISPLAY_USE_LCD=0 --define=BOARD_DISPLAY_USE_UART=1 --define=BOARD_DISPLAY_USE_UART_ANSI=1 --define=CC2640R2_LAUNCHXL --define=CC26XX --define=CC26XX_R2 --define=ICALL_EVENTS --define=ICALL_JT --define=ICALL_LITE --define=ICALL_MAX_NUM_ENTITIES=6 --define=ICALL_MAX_NUM_TASKS=3 --define=ICALL_STACK0_ADDR --define=POWER_SAVING --define=RF_SINGLEMODE --define=STACK_LIBRARY --define=USE_ICALL --define=xdc_runtime_Assert_DISABLE_ALL --define=xdc_runtime_Log_DISABLE_ALL -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi " "../TOOLS/app_ble.cfg"
TOOLS/subdir_rules.mk:12: recipe for target 'build-1287780815-inproc' failed
C:/Users/JONSW~1/AppData/Local/Temp/make8016-1.sh: Can't open C:/Users/JONSW~1/AppData/Local/Temp/make8016-1.sh: No such file or directory
C:/ti/xdctools_3_50_04_43_core/packages/xdc/bld/xdc_rules.mak:307: *** Error: Specified build configuration file '' is not found. Stop.
js: "C:/ti/xdctools_3_50_04_43_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[1]: *** [build-1287780815-inproc] Error 1
TOOLS/subdir_rules.mk:9: recipe for target 'build-1287780815' failed
gmake: *** [build-1287780815] Error 2
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

I am using the latest Windows 10 Pro

CCS version 7.4.0.00015

How can I fix this?