This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Failed to start Resource Explorer



Tool/software: Code Composer Studio

I have installed CCS7.4.0.00015_win32 I have installed using offline installer.

I am using windows 10 64 bit

my problem is "Failed to start Resource Explorer"

In the error details it shows that, "java.lang.nullpointerexception"

I think it has something to do with java

Please help me in finding the solution.

  • Hi Jagadeshwar,

    Please post the following log files

    • <ccs_workspace_folder>\.metadata\.log
    • c:\Users\<user_name>\ti\tirex-localserver-3.1.3\.logs

    Thanks,

    Oliver

  • thank you very much for replying

    i installed ccsv6 and trying to do my project in matlab

    now i dont have any problem with software

    but i am facing the following problem in matlab

    I am using a TI F28379D launchpad. I am a beginner. I have successfully installed the embedded support for C2000 in my laptop. While trying to execute the c2807x_2837xx_adcpwmasynctest_ert.slx example code on my pc I am facing a problem. The code is successfully build and downloaded into the target device. I can see a 390 HZ rectangular wave in my oscilloscope. But the problem is the pulse width of the wave is not changing with the adc input supplied to the ADCINA0 Pin30.

    I am using a 5V RPS to supply varying input voltage to PIN30. The value of the gain in the simulink model is 10

    I observe that when the voltage from the RPS increases more than 3.5 V the led lights on the board become brighter. This makes me feel that I have something to do with the board.

    I am unable to plot the data from the board in the simulink.

    Please help me to solve this problem.

  • Jagadeshwar,

    Sorry that this reply got missed. I see that you did start another post for this question in the C2000 device forum which is the correct place for it. We will go ahead and close out this thread.