Other Parts Discussed in Thread: C2000WARE, SFRA,
Tool/software: Code Composer Studio
I've installed CCS v7.4 on a Mac running OS 10.13.3. I've also downloaded and installed C2000ware and C2000ware digital power sdk. Both show up in the resource explorer. When I open an example project from the resource explorer the main.cfg file just shows up as a blank screen. When I installed CCS on a windows machine I had to install the GUI composer runtime to get everything to work, but on my Mac install I don't see any option to install the gui composer runtime in the CCS app center. Is there a way to install the GUI composer runtime on a Mac?
Also, when I try to start the compensation designer GUI and SFRA GUI nothing happens. I don't know if this is a related issue or not.