Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28069ISO
Tool/software: Code Composer Studio
We have just bought XDS110 debug probe to connect with JTAG connector on DRV8301-69M-KIT, but testing the connection results in an error. The in-built XDS100 of a control-card proved to be working with no issues.
Environment configuration:
- DEBUG port on XDS110 connected to JTAG 14-pin header on the kit via appropriate adaptor (the debug probe connected to the PC with originally provided USB cable)
- CCS version: 7.2.0.00013
- Changes in target configuration file: connection set to "Texas Instruments XDS110 USB Debug Probe"
- JTAG TCLK Frequency set to 1.0MHz (tried 100.0 kHz too with no difference).
The result I get after running the "Test Connection" button:
C:\Users\Jakub\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Dec 11 2017'.
The library build time was '12:04:14'.
The library package version is '7.0.100.1'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Texas Instruments XDS110 USB Debug Probe_0]
Attaching my target configuration file below:
/cfs-file/__key/communityserver-discussions-components-files/81/TMS320F28069_5F00_xds100v2.ccxml.txt
I have already found a few topics touching this issue, but the clues already given don't make any difference to me. For reference:
- https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/228782
- https://e2e.ti.com/support/wireless_connectivity/proprietary_sub_1_ghz_simpliciti/f/156/t/614015
- https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/628509/2333828#2333828
- https://e2e.ti.com/support/microcontrollers/c2000/f/902/t/607495