Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I'm beginner with Code Composer Studio, and I'm trying to do exercises from ssqc019 tutorial (C2000 Teaching ROM).
But following the instructions in Module_03 I'm unable to start code from Ram memory of my Experimenter's Kit Delfino.
1. Ubuntu 14.04.LTS x64
2. No anti-virus
3. Code Composer Studio Version: 7.4.0.00015
4. F28335 controlCard RELEASE 2.2 on Dockin-Stn USB-EMU [R3]
5. Problem description.
I'm trying to run simple program from RAM on F28335 Delfino Experimenter's Kit.
->New->CCS Project
Target: Experimenter's - Kit Delfino F28335
Connection: Texas Instruments XDS 100v1 Debug Probe (or XDS 100v2 debug probe)
In case of both probes verification is Ok.
Project name: Test3
Compiler version: Ti v16.9.6LTS
Output type: Executable
Output format: legacy COFF
Linker command file: 28335_RAM_lnk.cmd
Runtime support library: rts 2800_fpu32.lib
Project templates and examples:
Empty project (with main.c)
->Finish
->Project->Properties
->C2000 Linker ->Basic Options
Set C system stack size: 0x400
->Ok
Then I'm writing program doing “nothing”
01 unsigned int k;
02 unsigned int i;
03
04 void main(void)
05 {
06 while(1)
07 {
08 for (i=0; i<100; i++)
09 {
10 k = i*i;
11 }
12 }
13 }
->Build 'Debug' for project 'Test3'
Building is finished without problems:
**** Build of configuration Debug for project Test3 ****
/home/piotr/ti/ccsv7/utils/bin/gmake -k -j 4 all -O
Building file: "../main.c"
Invoking: C2000 Compiler
"/home/piotr/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --include_path="/home/piotr/workspace_CCSv7/Test3" --include_path="/home/piotr/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/include" --advice:performance=all -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
Finished building: "../main.c"
Building target: "Test3.out"
Invoking: C2000 Linker
"/home/piotr/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --advice:performance=all -g --diag_warning=225 --diag_wrap=off --display_error_number -z -m"Test3.map" --stack_size=0x400 --warn_sections -i"/home/piotr/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/lib" -i"/home/piotr/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.6.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="Test3_linkInfo.xml" --rom_model -o "Test3.out" "./main.obj" "../28335_RAM_lnk.cmd" -lrts2800_fpu32.lib
<Linking>
Finished building target: "Test3.out"
**** Build Finished ****
->Debug As Code Composer Debug Session
Program is loaded into RAM memory and execution stops before for (i=0; i<100; i++) instruction, blue arrow appears in line number 8. Then I'm able to push Step Into (button F5) and one line of code is executed from RAM. I can keep pushing F5 and code executes in steps. I can observe values of variables i and k in Expressions tab. In the Disassembly window I see my program and my instructions. When I try to run the code by clicking Resume (F8) it starts code execution from Flash memory. In my case two leds: LD1 and LD2, starts blinking on the control card. The program with blinking led diodes is flashed and starts on powering on the device. After pushing F8 button it is possible to Suspend (Alt+F8) the program but the content of Disassembly window is different. There is no my program with for loop increasing i variable.
How can I run code from Ram?
What should I checked?
–
Best Regards
Piotr