Part Number: MSP430F1611
Tool/software: TI C/C++ Compiler
Dear all,
my msp430f1611, I am trying to compile a C code that uses a header of .cpp.
When I try to compile it using sconscript, I get an error saying that unknow type name 'class', I have google this issue and yet, still haven't really figured out how to go about with this.
I attached codes on here, any help will be greatly appreciated.
Thank you
Kind regards
Yong Kim
#include "board.h"
#include "IpMtWrapper.h"
#include "dn_ipmt.h"
struct IpMtWrapper *ipmtwrapper;
//========================== "variables" ===================================
//===================== "functions declarations" ==============================
void timeIndication_Cb(dn_ipmt_timeIndication_nt* timeIndication);
void init_board(void);
//=========================== "main" ==========================================
int main(void) {
ipmtwrapper.setup(timeIndication_Cb);
}
void loop() {
ipmtwrapper.loop();
}
//=========================== "functions" =====================================
void timeIndication_Cb(dn_ipmt_timeIndication_nt* timeIndication) {
uint32_t elapsed_since_trigger;
uint32_t time_to_next_flip_reset;
uint32_t time_to_next_time_n_trigger;
uint32_t utcSecs;
uint32_t now;
//calculate_new_drift(timeIndication);
dn_read_uint32_t(&utcSecs, &timeIndication->utcSecs[4]);
//elapsed_since_trigger = static_cast<uint32_t> (nano_clock.ticksToNanos(static_cast<uint64_t> (nano_clock.getClockTicks() - last_trigger_timerTimestamp))/1000.);
//time_to_next_flip_reset = (1000000 - timeIndication->utcUsecs - elapsed_since_trigger)*drift_coef;
//pin_flipper.scheduleReset(time_to_next_flip_reset, drift_coef);
// TODO: this line is not working well. Do something about it
now = (utcSecs*1000*1000 + timeIndication->utcUsecs + elapsed_since_trigger)%(SYNCHRONIZATION_RATE*1000*1000);
uint32_t OFFSET = 0;
time_to_next_time_n_trigger = static_cast<uint32_t> ((SYNCHRONIZATION_RATE)*1000*1000 - now)*drift_coef;
if (SYNCHRONIZATION_RATE*1000*1000 - now < OFFSET*1000*1000) {
time_to_next_time_n_trigger += SYNCHRONIZATION_RATE*1000*1000;
}
reschedule_timer_n_timer(time_to_next_time_n_trigger);
}
//brief This function is called when the TimerA interrupt fires.
#pragma vector = TIMERA0_VECTOR
__interrupt void TIMERA0_ISR (void) {
P2OUT ^= 0x08; // toggle P2.3 - trig
__delay_cycles(250);
P2OUT ^= 0x08;
last_trigger_timerTimestamp = nano_clock.getClockTicks();
}
/*
void setup_time_n_timer() {
SimpleTimer::setCallback(4, time_n_trigger_handler);
SimpleTimer::configure(4, 2, 5*42*1000*1000);
SimpleTimer::start(4);
}
void reschedule_timer_n_timer(uint new_periode_us) {
SimpleTimer::configure(4, 2, new_periode_us*42);
SimpleTimer::start(4);
}
void calculate_new_drift(dn_ipmt_timeIndication_nt* timeIndication) {
static uint32_t last_sync;
uint32_t utcSecs;
double new_drift;
dn_read_uint32_t(&utcSecs, &timeIndication->utcSecs[4]);
// calculate deltas;
local_delta = nano_clock.ticksToNanos(static_cast<uint64_t> (last_trigger_timerTimestamp - last_sync))/1000.;
source_delta = static_cast<double> ((utcSecs - last_source_secs)*1000*1000 + timeIndication->utcUsecs - last_source_usecs);
if (last_source_secs != 0 && last_source_usecs != 0) {
drifter.addSyncData(local_delta, source_delta);
new_drift = drifter.processSyncData();
if (new_drift != 0) {
Serial.print("New drift: ");
Serial.println((new_drift-1)*1000000);
drift_coef = new_drift;
}
}
Serial.print("delta utcSecs: ");
Serial.println(utcSecs-last_source_secs);
Serial.print("delta utcSecs: ");
Serial.print(timeIndication->utcUsecs-last_source_usecs);
Serial.print(" ");
Serial.println(last_source_usecs - timeIndication->utcUsecs);
last_sync = last_trigger_timerTimestamp;
last_source_secs = utcSecs;
last_source_usecs = timeIndication->utcUsecs;
} */