Part Number: TDA3LA
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI C/C++ Compiler
Hello,
I am getting very strange linker issue. I have paste the linker issue here.
The problem is some how linker is not able to invoking the correct path for file search. The actual path is Debug/tmp/tmp/tmp//../../../common/source/drivers/DrvSpinlock/SpinlockDrv.obj"
instead of this, linker is invoking debug/tmp/tmp/tmp//../../../common/source/drivers/DrvSpinlock/SpinlockDv.obj" Means somehow linker got wrong file name. r is missing. Its very strange and i am fed up with this for a week to resolve this issue.
Please help me ASAP.
P. S. I am using CCS7.3. SpinlockDrv.obj is there in in specified path.
<Linking>
"C:\\Users\\npatel\\AppData\\Local\\Temp\\605443", line 138: error #10008-D: cannot find file "./Debug/tmp/tmp/tmp//../../../common/source/drivers/DrvSpinlock/SpinlockDv.obj"
>> Compilation failure
undefined first referenced
symbol in file
--------- ----------------
TSpinlockDrv::Init() ./Debug/app/Framework.obj
TSpinlockDrv::Take(TSpinlockId) ./Debug/app/Framework.obj
TSpinlockDrv::Release(TSpinlockId) ./Debug/app/Framework.obj
TSpinlockDrv::TSpinlockDrv() ./Debug/app/Framework.obj
TSpinlockDrv::~TSpinlockDrv() ./Debug/app/Framework.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Debug/m4_0.out" not built
gmake: *** [Debug/m4_0.out] Error 1
14:07:32 Build Finished (took 3s.432ms)
Best regards,
Naresh