Tool/software: Code Composer Studio
Hello!
Is it possible to hook into the dslite -executed commands in a way to override the power on/off requests with an external command? We are considering using the stand-alone Uniflash command line to do some automatic downloads but need to manually toggle the lines in reaction to script progress (or will need to create a parser for the command line output and supply input programmatically.) I see the program reacts differently to when the port is a stand-alone serial port vs. the XDS/FTDI ports already, so I assume there is a way to specify that.
How to adapt dslite to programmatically power on/off a board?