Part Number: TMS320F280049M
Tool/software: TI C/C++ Compiler
Hi Team,
My Customer using LTS16.9.3 asTMS320F280049 compiler in digital power control, while in different optimizer level, the power module acting as different way. with optimizer -off, the power module worked as normal, but with -o2/-3, the power module doesn't worked, now has configured the control related file and CLA related file optimization level as -off while the project setting as -o2/-3, the power module worked well, and also has provided the "Assembly language tools user's guide" to customer.
Need your team kindly support on below items:
1) Guides for C language coding, especially for variable definition/structure definition/pointer usage,
2) Application notes for how to implement the optimization level;
3) comments on customers' project properties;
Below is the project properties:
C2000 Compiler
-v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 -O3 --include_path="D:/Projects/OBC11kW/trunk/Primary_PFC1/PFC1_INV_BDC_APP_SVN48323_20180206_05_op" --
--advice:performance=all --define=DEBUG --define=_FLASH --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number
C2000 Linker
-v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 -O3 --advice:performance=all --define=DEBUG --define=_FLASH --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number -z -m"OBC_APP.map" --heap_size=0x200 --stack_size=0x400 --warn_sections -i"D:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.3.LTS/lib" -i"D:/ti/ccsv7/tools/compiler/ti-cgt-c2000_16.9.3.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="OBC_APP_linkInfo.xml" --entry_point=code_start --rom_model
Expect for your reply, thanks.
Best Regards
Benjamin