Part Number: TMS320C6713B
Tool/software: TI C/C++ Compiler
Hi
I see a strange behaviour of the compiler when I compile my code on our build server.
The error message I get is this
While compiling ..\GSI_App\Vmpg_if\TurbineIF\TurbineIF.c ->build\release_cc_tms6x\_pooma\LSI_fdsp\TurbineIF.obj command:'mkdir "build\release_cc_tms6x\_pooma\LSI_fdsp"2>NUL & C:\ti\ccsv6\tools\compiler\C6000_7.4.12\bin\cl6x -k -al -pr -pden -mv6710 --gen_func_subsections=on -pm -pdsr232 -pdsr383 -pdsr1 -pden -O3 --symdebug:skeletal -i"C:\ti/ccsv6/tools/compiler/c6000_7.4.12/include" -i"C:\ti/bios_5_42_02_10/packages/ti/bios/include" -i"C:\ti/C6xCSL/include" -i"C:\ti/xdctools_3_22_04_46/packages" -i..\GSI_App\Appl -iAppl\ApplConfig -i..\GSI_App\Appl\ApplConfig -iCtrllLib -i..\..\SignalBlockManager\sbm_runtime\include -i..\GSI_App -i.. -i..\GSI_App\Appl\Common -i..\GSI_App\MSC\MSC_CTRL -i..\GSI_App\CPL\PlatformSupport -i..\GSI_App\CPL\PlatformSupport\PlatformIO -i..\GSI_App\CPL\driver -i..\GSI_App\CPL -i..\GSI_App\Appl\dspbios -i..\GSI_App\CPL\PlatformSupport\Flexpower -i..\GSI_App\CPL\PlatformSupport\Flexpower\DriverConfig -i..\..\Conv_Framework\if -i..\..\Conv_Framework\if\dspbios -i..\..\Conv_Framework -i..\..\Conv_Framework\driver -i..\..\Conv_Framework\dspbios\CT_460 -i..\..\Conv_Framework\IO_Common -i..\..\Conv_Framework\IO_FLEX -i..\..\Conv_Framework\Services -i..\..\Conv_Framework\Services\ParamManager -i..\..\Conv_Framework\OldLibs\CFC -d_DSPBIOS -dCHIP_6713 -d_HS_SECTIONS -d_CT_460 -d_SM_DEBUG -dDATASPACE_SERVER -dGDS_REPLICATION_ENABLED -dBENCH_MANUAL_CONTROLS -fsbuild\release_cc_tms6x\_pooma\LSI_fdsp -frbuild\release_cc_tms6x\_pooma\LSI_fdsp ..\GSI_App\Vmpg_if\TurbineIF\TurbineIF.c' output:' <Optimizing> (Local CPU 7) <Generating> <Assembling> "build\release_cc_tms6x\_pooma\LSI_fdsp\TurbineIF.asm", ERROR! at line 39: [E0300] Cannot equate an external symbol to an external symbol _TurbineIF_Handle .set _TurbineIF_EventHandler "build\release_cc_tms6x\_pooma\LSI_fdsp\TurbineIF.asm", ERROR! at EOF: [E0300] The following symbols are undefined: 2 Assembly Errors, No Assembly Warnings _TurbineIF_EventHandler Errors in Source - Assembler Aborted >> Compilation failure
Then If I just recompile without changing anything, the compilation does not fail.
The assembler file TurbineIf.asm is the same whether it fails or not
and the part where it reports an error looks like this
;******************************************************************************
;* TMS320C6x C/C++ Codegen PC v7.4.12 *
;* Date/Time created: Tue Feb 13 13:26:22 2018 *
;******************************************************************************
.compiler_opts --abi=coffabi --c64p_l1d_workaround=default --endian=little --hll_source=on --long_precision_bits=40 --mem_model:code=near --mem_model:const=data --mem_model:data=far_aggregates --object_format=coff --silicon_version=6710 --symdebug:skeletal
;******************************************************************************
;* GLOBAL FILE PARAMETERS *
;* *
;* Architecture : TMS320C671x *
;* Optimization : Enabled at level 3 *
;* Optimizing for : Speed *
;* Based on options: -o3, no -ms *
;* Endian : Little *
;* Interrupt Thrshld : Disabled *
;* Data Access Model : Far Aggregate Data *
;* Pipelining : Enabled *
;* Speculate Loads : Enabled with threshold = 0 *
;* Memory Aliases : Presume are aliases (pessimistic) *
;* Debug Info : DWARF Debug for Program Analysis w/Optimization *
;* *
;******************************************************************************
.asg A15, FP
.asg B14, DP
.asg B15, SP
.global $bss
$C$DW$CU .dwtag DW_TAG_compile_unit
.dwattr $C$DW$CU, DW_AT_producer("TMS320C6x C/C++ Codegen PC v7.4.12 Copyright (c) 1996-2014 Texas Instruments Incorporated")
.dwattr $C$DW$CU, DW_AT_TI_version(0x01)
.dwattr $C$DW$CU, DW_AT_comp_dir("D:\B\CON-CFLEXIB-JOB1\converter\FlexInvert_Appl\FLEXInvert_Appl")
;*****************************************************************************
;* FUNCTION SYNONYMS *
;*****************************************************************************
.global _TurbineIF_Handle
_TurbineIF_Handle .set _TurbineIF_EventHandler
.global _TurbineIF_Handle_Scan
_TurbineIF_Handle_Scan .set _TurbineIF_Scan$0
;*****************************************************************************
;* CINIT RECORDS *
;*****************************************************************************
.sect ".cinit"
.align 8
.field 4,32
.field _TurbineIF_evtHandle+0,32
.bits 0,32 ; _TurbineIF_evtHandle @ 0
.sect ".cinit"
.align 8
.field 4,32
.field _eTaskState$0+0,32
.bits 1,32 ; _eTaskState$0 @ 0
More info:
We compile from command line, and we use compiler version C6000_7.4.12.
It seems that the error only happens on our build server, and not if we build on our own PC, even though the installation on the build servers is identical to the one on our PC's.
We use Incredibuild to speed up the compilation - both on build server and from our own PC.
Any ideas on what causes this error and how to avoid it?
Best
Jens