This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P4011: MSP432P4111 LaunchPad Development OOB, project from Cloud CCS will not activate...

Part Number: MSP432P4011

Tool/software: Code Composer Studio

Hello!,

Working today with the OOB demo code for the MSP432P4111 Launchpad.  Compiles fine with TI Cloud IDE, but when I export it to the local machine, when I bring the project into CCS, Ino error) it will not activate.

I guess my question is what else do I need to do to test locally.

Yes, I have the correct Simplelink SDK in the C:\ti directory.

The cloud exported project is another directory called "C:\Codetest|TIEco\"

Thanks, in advance for your comment.

Randy

  • Rando said:
    I guess my question is what else do I need to do to test locally.

    Rather than exporting from Cloud and importing into your desktop CCS, you can simply import the OOB demo project directly from Resource Explorer on the desktop CCS. If you already have Simplelink MSP432P4 SDK installed, then you should just be able to expand down to the example and click on the icon to Import to IDE.

    Please let me know if this helps with what you are looking to do.