Part Number: LAUNCHXL-CC1352R1
Tool/software: Code Composer Studio
Hi,
During a debug session with the CC1352R1 launchpad I periodically get the error message:
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 7.0.100.1)
I am not using IcePick as far as I know (in the debug config it is written as Cortex_M4_0. I can fully debug the device, but when it shows this error code composer freezes for a few seconds which makes it a bit hard to work with.
Would appreciate some help with this
Thanks