Part Number: CC1352R
Tool/software: TI C/C++ Compiler
Hi
I am trying to compile an inline assembly code ,listed below.
This code is taken from an open source to optimize an existing C code.
static inline spx_word32_t MULT16_32_Q14(spx_word16_t x, spx_word32_t y) {
int res;
int dummy;
asm (
"smull %0,%1,%2,%3 \n\t"
"mov %0, %0, lsr #14 \n\t"
"add %0, %0, %1, lsl #18 \n\t"
: "=&r"(res), "=&r" (dummy)
: "r"(y),"r"((int)x));
return(res);
}
#undef MULT16_32_Q15
static inline spx_word32_t MULT16_32_Q15(spx_word16_t x, spx_word32_t y) {
int res;
int dummy;
asm (
"smull %0,%1,%2,%3 \n\t"
"mov %0, %0, lsr #15 \n\t"
"add %0, %0, %1, lsl #17 \n\t"
: "=&r"(res), "=&r" (dummy)
: "r"(y),"r"((int)x));
return(res);
}
#undef DIV32_16
static inline short DIV32_16(int a, int b)
{
int res=0;
int dead1, dead2, dead3, dead4, dead5;
__asm__ __volatile__ (
"\teor %5, %0, %1\n"
"\tmovs %4, %0\n"
"\trsbmi %0, %0, #0 \n"
"\tmovs %4, %1\n"
"\trsbmi %1, %1, #0 \n"
"\tmov %4, #1\n"
"\tsubs %3, %0, %1, asl #14 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #14 \n"
"\tsubs %3, %0, %1, asl #13 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #13 \n"
"\tsubs %3, %0, %1, asl #12 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #12 \n"
"\tsubs %3, %0, %1, asl #11 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #11 \n"
"\tsubs %3, %0, %1, asl #10 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #10 \n"
"\tsubs %3, %0, %1, asl #9 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #9 \n"
"\tsubs %3, %0, %1, asl #8 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #8 \n"
"\tsubs %3, %0, %1, asl #7 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #7 \n"
"\tsubs %3, %0, %1, asl #6 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #6 \n"
"\tsubs %3, %0, %1, asl #5 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #5 \n"
"\tsubs %3, %0, %1, asl #4 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #4 \n"
"\tsubs %3, %0, %1, asl #3 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #3 \n"
"\tsubs %3, %0, %1, asl #2 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #2 \n"
"\tsubs %3, %0, %1, asl #1 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4, asl #1 \n"
"\tsubs %3, %0, %1 \n"
"\tmovpl %0, %3 \n"
"\torrpl %2, %2, %4 \n"
"\tmovs %5, %5, lsr #31 \n"
"\trsbne %2, %2, #0 \n"
: "=r" (dead1), "=r" (dead2), "=r" (res),
"=r" (dead3), "=r" (dead4), "=r" (dead5)
: "0" (a), "1" (b), "2" (res)
: "cc"
);
return res;
}
I get errors on the first line in each asm block which starts with ':' sign (colon).
The error is " #18 expected a ")" " , Imust stress that the number of brackets is balanced.
It seems that the compiler is fine with the code itself but not with the directions below it .
Can someone advice.
Regards
Nitzan Tzifroni