Part Number: CC1310
Hi,
I need to automatically updated the CC1310 existing firmware in the internal flash.I Stored the updated image in the external flash. once the boot loader identify the updated image in the external flash and boot loader is to replace the firmware which is present in the internal flash with stored updated image(available in external flash). please any one give some suggestions to implement same.
Thanks and regards,
Arunraj K.