Other Parts Discussed in Thread: TMS320C6472
I've recently purchased/received the TMS320C6472 Evaluation Module. It came with a DVD of code composer studio v4.1.2, which I had trouble when installing from the DVD.
During the installation process, I chose a custom install and selected "only provide code for C6000 devices". Towards the end of the install I got an error that said the installer couldn't make a backup copy evmc6472.bat. It was trying to make this backup on the DVD drive. I had to move the entire installation folder from the DVD drive to the C: drive and run it from there. It installed without complaint from the C drive.
Now I'm new to CCS, and I'm not certain that the DVD that came with the eval module is the "out of the box" version of CCS, because the DVD appears to have software specific to the eval module. So perhaps this problem will affect very few, but I thought I'd mention it.