This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Can't install CCS7.4.0.00015_linux-x64 on linux 14.04

Genius 13655 points

Tool/software: Code Composer Studio

Hello Champs,

Customer can't install CCS7.4.0.00015_linux-x64 on linux 14.04, below is the installation log. 

Is it a bug for ccs 7.4?

21:07:31] DEBUG_x64: Changing File Permissions 755 (common/uscif, emulation/drivers, emulation/Blackhawk/Install)
LINUX
[21:07:31] DEBUG: USCIF.OUT exists or BHUSCIF.OUT does not exist.
[21:07:31] DEBUG: BHUSCIF.OUT does not exist to clean up.
Creating Uninstaller
Creating uninstaller 25%
Creating uninstaller 50%
Creating uninstaller 75%
Creating uninstaller 100%
Installation completed
LINUX
[21:07:32] DEBUG: Changing File Permissions 755 (uninstallers: /opt/ti/ccsv7/uninstallers/{uninstall_bh_emupack})
[21:07:32] DEBUG: Changing File Permissions 666 (log file: /tmp/bitrock_installer_18305.log)
[21:07:32] DEBUG: Running script to install device driver RULES file.
Executing /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install
Script exit code: 1

Script output:
bh usb560 installation completed successfully. Some versions of Linux
require a reboot in order for the driver to function properly. For other
versions restarting udev is sufficient. Restarting udev now ...
ERROR: failed to restart udev, reboot required

Script stderr:
stop: Unknown job: udev
start: Unknown job: udev

Error running /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install: stop: Unknown job: udev
start: Unknown job: udev
Problem running post-install step. Installation may not complete correctly
Error running /opt/ti/ccsv7/ccs_base/emulation/Blackhawk/Install/bh_driver_install.sh --install: stop: Unknown job: udev
start: Unknown job: udev
179,1 97%

Thanks.
Rgds
Shine