This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: when import CCS3.3 prj to CCS7, occured "cannot open source file "std.h" "

Tool/software: Code Composer Studio

Someone help please,

Using Import Legacy CCSv3.3 Project feature in order to made CCS7 environment.

But happened 1 thing error, cannot open source file "std.h"

Resetting properties(General -> Project -> Variant, General-> Product->DSP/BIOS, XDAIS, XDCtools) and then change path, C2000 Include Option.

There is remaining.. Im so confused 

help me

  • Information on the reason for this diagnostic and how it can be fixed is in this page.

    If you are using DSP/BIOS there may some other factors involved as well. In your CCSv7 environment do you have it set up to use the same version of DSP/BIOS as was used with CCS 3.3?

    To isolate the issue further, you could find the compiler and BIOS build options used in the CCS 3.3 project and ensure that they match up with the options in the CCSv7 project.

  • Thanks AartiG

    I'm solved this problem that need old version (install c2000 5.2.1) Complier