Tool/software: Code Composer Studio
Running Linux 64-bit with all the necessary 32-bit libraries installed and trying to install CCS 6.1.1.00022!!! Installer initial library check does not complain so it can find all of them.
I have tried both offline and web installer, both fail at the same point.
The failure point is the download of file ti_dspack_ibsetup_6.1.0.1349.bin, relevant log entry:
processOtherFeatures - ti_dspack_ibsetup_6.1.0.1349.bin does not exist at /home/dari/.ccsv6/ccsv6/eclipse/downloads/ti_dspack_ibsetup_6.1.0.1349.bin. Setting state to feature downloaded
This is clearly an issue with your software repository.
Please put that file online again!
And please don't suggest to upgrade to CCSv7 or CSv8, I can't. It's a hard requirement for me to use that exact version.
Thanks!