Part Number: CCSTUDIO
Other Parts Discussed in Thread: MSP430F67771
Tool/software: Code Composer Studio
Hello,
I am working with CCS 7.4 and with an imported makefile project. The target is an ARM M4 of the TDA3. The Project uses the compiler ti-cgt-arm_5.2.5 from VSDK 2.8. In the build options the error parsers are activated.
If a compiler error occures, there is no error highlightning in the console and therefore no jump to the apropriate source position is possible. Same project with CCS 5.5 recognizes the errors and a jump is possible.
Is it a bug or do I have to configure something?
Best regards,
Milan