Other Parts Discussed in Thread: OMAP-L138
I have two customers who have purchased CCSv3.3 licenses that would like to upgrade to v4.x. Where should I point them in order to make this happen? It is my understanding that this is possible.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138
I have two customers who have purchased CCSv3.3 licenses that would like to upgrade to v4.x. Where should I point them in order to make this happen? It is my understanding that this is possible.
Ki-Soo,
I was just helping a customer through this today and found this post. Is this the proper procedure if a customer purchases, for example, an OMAP-L138 EVM from LogicPD which comes with CCSv3.3 and they want to upgrade to CCSv4.x? If this is true, IMHO, this is as easy as it gets - the right solution for our users - as long as they can FIND IT.
One other side note, gee, it sure would be helpful if our 3rd parties had a bright "red" card that shipped in the box that said "IF YOU WANT TO UPGRADE TO A LATER VERSION OF CCS, DO THIS...". Or, maybe that is already happening. If not, I can just imagine our customers spending useless cycles trying to locate the info in your post above.
Thanks a bunch,
Eric
Hi Eric,
eric_wilbur said:Is this the proper procedure if a customer purchases, for example, an OMAP-L138 EVM from LogicPD which comes with CCSv3.3 and they want to upgrade to CCSv4.x?
If they have an EVM version of CCS and are using the onboard emulation of the L138 EVM, they can simply request a free bundled license and use that with v4. No need to e-mail that e-mail list.
If they have a full CCS version with a valid subscription, and did not automatically get an activation code, then they should e-mail the list as mentioned above. This is also described here:
http://processors.wiki.ti.com/index.php/Licensing_-_CCSv4#Upgrading_to_CCS_v4
eric_wilbur said:One other side note, gee, it sure would be helpful if our 3rd parties had a bright "red" card that shipped in the box that said "IF YOU WANT TO UPGRADE TO A LATER VERSION OF CCS, DO THIS...". Or, maybe that is already happening. If not, I can just imagine our customers spending useless cycles trying to locate the info in your post above.
I'm not sure how these kits are packaged. But I would imagine that if they are coming with CCSv3.3, then there is no resource about upgrading to v4 (could be that the kits were put together before v4 was available).