This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320C6678: just fit size doesn't work with cgt 8

Part Number: TMS320C6678

Tool/software: TI C/C++ Compiler

.vects needs just 16 * 0x20 == 0x200 bytes, 

I put it at the MSMC's tail 0x200 bytes , an error occurs when link with cgt v8.2.2

-------------------------------------------------------------------------------------------------------

"../MCBL.cmd", line 35: error #10099-D: program will not fit into available
memory. placement with alignment fails for section ".vecs" size 0x200 .
Available memory ranges:
VECTORS size: 0x240 unused: 0x240 max hole: 0x240
error #10010: errors encountered during linking; "MCBL.out" not built

--------------------------------------------------------------------------------------------------------

I tried  a larger size like 0x240, it doesn't work until a largerrr size like 0x400.

it's ok when i use cgt v7.4.24, 0x200 is enough.