Other Parts Discussed in Thread: SEGGER
Tool/software: Code Composer Studio
I am using the following:
- CCS version 8.0.0.00016
- Segger J-Link Plus (with latest f/w update as of this afternoon)
- DK-TM4C129X dev kit
- Windows 10 (X64)
I was trying to get a simple sample project using Micrium's uC/OS-II working on my setup. I experienced a problem where in the RTOS' assembly code that launches the startup task, the address of the startup task was not getting loaded properly into a register. After working with Micrium tech support, we discovered that there seems to be a problem when using the J-Link debugger.
There is a line of code in the RTOS that consists of an “MSR CONTROL, R0” instruction. That instruction should result in bit 1 of the CONTROL register being set. However, when using the J-Link, the bit does not get set. If I use the ICDI debug interface, it works fine.
I also discovered that if I use the J-Link, and do a CPU Reset before executing, the code also works correctly.
This seems to indicate that something is going on when the J-Link debugger is loading the memory and getting things initialized that is preventing the CONTROL register from being properly accessed. Resetting the CPU appears to fix things.
I have zipped up the project files and made them available on Dropbox at the following link: https://www.dropbox.com/s/hjqew6icu7tk2e4/VIO-CPU-Port.zip?dl=0.
The specific line of code that does not work is line 238 of os_cpu_a.asm
I appreciate any help you can give me regarding this issue.
Regards,
Dave