I am trying to connect to the DSP on the DM6467 EVM.
In the ccxml file, I have chosen
Connection: Spectrun Digital XDS510 Parallel Port-PCI Emulator
Board: evmDM6467.
In advanced, I have bypassed all the ARM configs.
So, when I connect to the DSP, I get
"Error connecting to the target:
Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration."
So, what exactly am I missing ??