Part Number: AM1707
Tool/software: Code Composer Studio
Support Path: /Tools & software/Help me with an issue/Design Kits / Evaluation Modules / Boards/Software issue/
I have located and downloaded the GEL file from Spectrum Digital, but I can't find any instructions for adding board support to CCS other than "re-run the installer and pick the board you want." CCS v6.2 supports the EVMAM1808, but not the EVMAM1707. I duplicated the EVMAM1808 directory structure as EVMAM1707 and placed the GEL in the appropriate subdirectory, but CCS doesn't recognize it. I have also located and downloaded a "board configuration" file from Spectrum Digital (filetype is ".ccs"), but cannot find any instructions for how to use that file. I opened the file to see if I could derive understanding from its contents, but they are binary with a few description strings, so that was not helpful.
I really don't want to have to install CCS v4 alongside my working v6.2 system just to support this eval board. Any help would be appreciated.