This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am converting this project and when I build a .cmd file is generated that produces build errors. We believe a .tcf file may be able to help but simply adding the .tcf file does not work. Is there some other file type that replaces .tcf and can we convert our current .tcf file to it? Do we need to do something else instead?
What worked for me, was migrate 3.3 project to 5.x, which supports both DSP/BIOS and SYSBIOS, then migrate to SYSBIOS and then upgrade CCS.
I downloaded and installed DSP/BIOS v5.4 and it did not seem to fix the problem either. Shouldn't I be able to use .tcf files with that installed? Same as before?