This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Missing support for Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator in Linux CCS release



Tool/software: Code Composer Studio

I'm using CCS 7.2 with C5517 EVM board under Windows and there is no problem. But now I need to use CCS for Linux.

I try to make setup as it is described at:

but I found missing full support for - Spectrum Digital Debug probes and Boards when try to create new -> Target configuration file. There is no support for Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator in the Connection combo box. See screen shot:

During CCS v8.0 installation I have added check for Spectrum Digital support.
Is it known issue for CCS for Linux releases or I'm missing something during installation?



BR
Tsvetolin Shulev