Part Number: MSP432P401R
Tool/software: TI C/C++ Compiler
Hi!
I'm trying to print 32 bits number (input) to the terminal. However, it didn't print anything (or maybe I do not know where to look for the output). I got warnings when I run the project. Below is the warning and I include the lines.
"../project_zero.c", line 1169: warning #225-D: function "printf" declared implicitly
case LED_CHAR1:
switch (PROFILE_ID_CHARTYPE(charID))
{
case PROFILE_VALUE:
//32 bits
LEDService_getParameter(charID, &value);
printf("%d\n", value);
break;
default:
break;
}
break;
"../Profile/led_service.c", line 501: warning #70-D: integer conversion resulted in truncation ".
case LED_CHAR1:
switch (PROFILE_ID_CHARTYPE(charID))
{
case PROFILE_VALUE:
if (len == sizeof(ls_LED0OnOFFVal))
{
memcpy((uint8_t *)&ls_LED032BitsVal, pData, sizeof(ls_LED032BitsVal));
status = SNP_SUCCESS;
notifyApp = LS_LED0_32BITS_UUID;
}
break;
./Profile/led_service.c", line 535: warning #169-D: argument of type "uint8_t" is incompatible with parameter of type "void *__restrict__" "..
/Profile/led_service.c", line 537: warning #70-D: integer conversion resulted in truncation
case LED_CHAR3:
switch (PROFILE_ID_CHARTYPE(charID))
{
case PROFILE_VALUE:
if (len == sizeof(ls_LED0SwitchVal))
{
memcpy(ls_LED0SwitchVal, pData, sizeof(ls_LED0SwitchVal));
status = SNP_SUCCESS;
notifyApp = LS_LED0_HA_INTENSTITY_UUID;
}
break;
Thanks,
Janna Razali