Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Dear all,
i have a simple Simulink code in which i have a UDP receive block for my concerto microcontroller. I have set through the settings, the IP for my microcontroller and i have placed its mask.
When i compile my code through Simulink it loads and runs perfect. More than that, i am able to successfully ping the microcontroller's IP through the command window.
When i load though the out file at CCS, at the moment i press run, CCS shuts down without giving any information on why is this happening. If the Ethernet cable is disconnected, and i press run it will run properly but when i will then connect the ethernet cable again it will imidiatell closed.
Can anyone help me with this?
ps: On the other side of the ethernet cable i have at the moment a switch on which my computer is also connected.
Thanks in advance.
Kind regards,
Alex