Part Number: TMS320F28335
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hello everybody
I want to create a PWM waveform with Simulink/MATLAB R2012a in DSP F28335. I'm using CCS v3.3 as described in this video:
Th problem is that after creation in MATLAB and receiving this message in MATLAB main window:
"
### Connecting to Code Composer Studio(tm) ...
Target Preferences block specifies that the board named '' will be used to run generated code.
However, since only board named 'F28335 XDS100 USB Emulator' is found in your system, that board will be used.
### Generating code into build folder: D:\Scientific\PHD\Proposal\Experimental\Code\PWMtest1_ticcs
Warning: Unable to determine a fixed step size
based on the sample times in the model 'PWMtest1',
because the model does not have any discrete
sample times. Picking a fixed step size of (0.2)
based on simulation start and stop times. You can
disable this diagnostic by explicitly specifying a
fixed step size in the Solver pane of the
Configuration Parameters dialog box, or setting
the 'Automatic solver parameter selection'
diagnostic to 'none' in the Solver group on the
Diagnostics pane of the Configuration Parameters
dialog box.
### Invoking Target Language Compiler on PWMtest1.rtw
### Using System Target File: C:\Program Files\MATLAB\R2012a\toolbox\idelink\foundation\pjtgenerator\rtw\idelink_ert.tlc
### Loading TLC function libraries
....
Warning: The data type "int8" uses a word size that is not available on the intended target.
Fixed-point signals using this data type will be put inside a larger word or multi words. When used,
extra software will be generated to force this larger word or multi words to emulate a smaller
word. This emulation is helpful when your prototype target and your final
production target are not the same. If the smaller word size does NOT exist
on the final production target, then consider increasing the word size to
one that is supported.
Warning: The data type "uint8" uses a word size that is not available on the intended target.
.
Warning: The data type "boolean" uses a word size that is not available on the intended target.
### Initial pass through model to cache user defined code
..
### Caching model source code
...............
### Writing header file PWMtest1.h
.
### Writing header file PWMtest1_types.h
### Writing header file rtwtypes.h
.
### Writing source file PWMtest1.c
### Writing header file PWMtest1_private.h
.
### Writing source file PWMtest1_main.c
### TLC code generation complete.
.### Creating project: D:\Scientific\PHD\Proposal\Experimental\Code\PWMtest1_ticcs\PWMtest1.pjt
### Project creation done.
### Building project...
>>
"
In CCS v3.3 environment I receive this errors and it doesn't work:
"
[DSP2833x_ADC_cal.asm] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_ADC_cal.asm"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_CodeStartBranch.asm] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_CodeStartBranch.asm"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_CpuTimers.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_CpuTimers.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_DefaultIsr.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_DefaultIsr.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_DMA.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_DMA.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_GlobalVariableDefs.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_GlobalVariableDefs.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_MemCopy.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_MemCopy.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_PieCtrl.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_PieCtrl.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_PieVect.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_PieVect.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_SysCtrl.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_SysCtrl.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[DSP2833x_usDelay.asm] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW.lkf" "DSP2833x_usDelay.asm"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[MW_c28xx_board.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"CustomMW.lkf" "MW_c28xx_board.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[MW_c28xx_csl.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"CustomMW.lkf" "MW_c28xx_csl.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[MW_c28xx_pwm.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"CustomMW.lkf" "MW_c28xx_pwm.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[PWMtest1.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"CustomMW.lkf" "PWMtest1.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[PWMtest1_main.c] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -fr"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs/CustomMW" -i"C:/Program Files/MATLAB/R2012a/toolbox/idelink/extensions/ticcs/inc" -i"D:/Scientific/PHD/Proposal/Experimental/Code/PWMtest1_ticcs" -i"D:/Scientific/PHD/Proposal/Experimental/Code" -i"C:/Program Files/MATLAB/R2012a/extern/include" -i"C:/Program Files/MATLAB/R2012a/simulink/include" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src" -i"C:/Program Files/MATLAB/R2012a/rtw/c/src/ext_mode/common" -i"C:/Program Files/MATLAB/R2012a/rtw/c/ert" -d"__TICCSC__" -d"RT" -d"USE_RTMODEL" -d"MODEL=PWMtest1" -d"NUMST=1" -d"NCSTATES=0" -d"HAVESTDIO=" -d"ONESTEPFCN=1" -d"TERMFCN=1" -d"MAT_FILE=0" -d"MULTI_INSTANCE_CODE=0" -d"INTEGER_CODE=0" -d"MT=0" -d"TID01EQ=0" -ml -v28 --float_support=fpu32 -@"CustomMW.lkf" "PWMtest1_main.c"
>> WARNING: invalid compiler option --float_support=fpu32 (ignored)
[Linking...] "C:\CCStudio_v3.3\C2000\cgtools\bin\cl2000" -@"CustomMW.lkf"
<Linking>
>> C:\Users\asus\AppData\Local\Temp\TI5763, line 19: error:
can't find input file 'rts2800_fpu32.lib'
>> Compilation failure
Build Complete,
2 Errors, 16 Warnings, 0 Remarks.
"
Does anybody have any idea?
I'd appreciate if someone can guide me.
Regards,
abolfazl