This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6000 cgtools v7.0.4 : Are there any issues with combing objects built with -mv6740 with ones built with -mv6400+

Compiler Team,

This question is with respect to C6000 cgtools v7.0.4. Are there any issues with combing objects built with -mv6740 along with ones built with -mv6400+ in a single project or library? For example, if we want to reuse a fixed point library built with -mv6400+ into a 'C674x project built with -mv6740, do we have to rebuild the libraries? Similarly, if we have fixed point library built with -mv6740, can we reuse this in a project built with -mv6400+?

Will this work? Are there any caveats or performance concerns?

Thanks