Part Number: MSP432P401R
Tool/software: TI C/C++ Compiler
I am using a temperature sensor (si7021) hooked up to an I2C port on the MSP432P401R launchpad. I am using TI-RTOS and the TI/CCS compiler. The code works.
I'd like to make a custom library, with a si7021.h and si7021.c file, to get all of the function declarations and functions themselves out of the main.c. In other compilers, I would just create a .h file with the declarations, and a .c file of the same name with the functions themselves, then include the header in main.c and call the functions in the program. This isn't working.
I get compiler errors every time my si7021.c tries to reference any I2C object from the I2C drivers that are referenced in the main.c file.
What am I missing?
Appreciate any assistance. I can include code, but figured this is probably something more fundamental.