Other Parts Discussed in Thread: AM3358
Tool/software: Code Composer Studio
I created a PRU AM3358 project on CCS and tryed to use `sprintf`, which use all my code memory. By standard the `AM335x_PRU.cmd` memory map file is:
/* Specify the System Memory Map */
MEMORY
{
PAGE 0:
PRU_IMEM : org = 0x00000000 len = 0x00002000 /* 8kB PRU0 Instruction RAM */
PAGE 1:
/* RAM */
PRU_DMEM_0_1 : org = 0x00000000 len = 0x00002000 CREGISTER=24 /* 8kB PRU Data RAM 0_1 */
PRU_DMEM_1_0 : org = 0x00002000 len = 0x00002000 CREGISTER=25 /* 8kB PRU Data RAM 1_0 */
PAGE 2:
PRU_SHAREDMEM : org = 0x00010000 len = 0x00003000 CREGISTER=28 /* 12kB Shared RAM */
DDR : org = 0x80000000 len = 0x00000100 CREGISTER=31
L3OCMC : org = 0x40000000 len = 0x00010000 CREGISTER=30
/* Peripherals */
... // I did put here because I though that this can't be modified.
}
Is it possible to change the `PRUY_IMEM` space to fit my code? Which manual have the "CCS MEMORY{ " directives? What are the limit?