Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hello,
We worked on the ControlCard for F28377 with integrated Xds100 probe.
Than after some time, we bought the XDS560v2 probe which work also properly.
We developed our custom board based on the F28377s. On this board, the Xds560v2 probe work properly.
Now, two develop with two people in the same time, we buy the Xds200 probe.
Then in the CCS (v7.4) project, we add the target configuration for this probe and try to debug with this configuration.
The probe is plugged on USB to the computer and on the JTAG on the target side. The Left Green led is light On, the right is light off
Then the configuration start correct
The Left AND Right are light on few time and the both are Light Off.
Then the CCS display following (The connection is not Ok, debug is not possible):
Is somebody can inform me about something to check?
Thank