Part Number: TMS320C6416
Other Parts Discussed in Thread: TMS320C6414, TMS320C6414T
Tool/software: Code Composer Studio
Hello,
I've been trying to debug the TMS320C6416T.. I do not have a project to load yet and i want to write it as i debug, so i have been trying to first connect to the DSP in debug mode.
Using the BLACKHAWK USB560v2 System Tracer and another BLACKHAWK-LAN-560 debugger, both succeed with not a single error doing the "Test Connection" yet they still throw the same error at me when trying
to "Connect to Target".. it says "Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver"
I have tried updating everything possible in many different versions for both of the debuggers mentioned above with no success...
Not sure what to do next .. can anyone help me understand what could possibly make me unable to connect to the DSP?
Thank you all in advance!