This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/PROCESSOR-SDK-AM437X: ROV of CCS 7.4.0.00015 does not work

Part Number: PROCESSOR-SDK-AM437X

Tool/software: Code Composer Studio

Hi,
I am using 'ti-processor-sdk-rtos-am437x-evm-04.03.00.05-Windows-x86' under Windows 7.

The ROV tool does. Refer to the picture.


ROV of PDK version 04.00.00.04 works well on the same machine, debugging the same aplication on the same custom board.

regards,
Marcio

  • Hi Marcio,

    Can you try ROV Classic? Does it work? If it does, you can use it. If it works, what version of XDCtools and SYS/BIOS are you using?

    Todd
  • Hi Todd,

    The ROV classic works ok.

    I have not realized that there are 2 versions of ROV. When I said the ROV works well with PDK version 04.00.00.04, was talking about the ROC Classic.

    The SYS/BIOS version is 6_52_00_12 and the XDCtools version is 3_50_04_43_core. They came with 'ti-processor-sdk-rtos-am437x-evm-04.03.00.05-Windows-x86'. The CCS is 7.4.0.00015_win32.

    Thanks you,
    Marcio.